Cancel
Showing results for 
Search instead for 
Did you mean: 

Error while installing Teamcenter 12

Solution Partner Creator Solution Partner Creator
Solution Partner Creator

"deploy_runner.bat" -u=infodba -p=***** -g=dba -templates=cla0classification -targetkit=X:\Setup\TC Setup\Teamcenter 12\TC12.0.0.0_wntx64_1of_2

1 REPLY 1

Re: Error while installing Teamcenter 12

Gears Phenom Gears Phenom
Gears Phenom

Good afternoon, among the reasons there may be spaces in your installation path:

 

Output from command:  "deploy_runner.bat" -u=infodba -p=***** -g=dba -templates=cla0classification -targetkit=X:\Setup\TC Setup\Teamcenter 12\TC12.0.0.0_wntx64_1of_2

The following arguments are not supported by this utility:

"Setup\Teamcenter,12\TC12.0.0.0_wntx64_1of_2".

Please refer to the usage below.

 

Usage:$TC_ROOT/bin/deploy_runner

      -u=<user id> -p=<password> -pf=<password file> -g=<group>

      [-path=<existing installation path>]

      -targetkit=<path to the Teamcenter media>

      -templates=<list of template names>

      [-log=<log file>] [-h]

 

This utility is used to deploy Teamcenter.

Options:

  -u=             Teamcenter user ID.

 [-p=             Teamcenter password associated with the -u=<user_id> argument.

|-pf]=            Teamcenter password file associated with the -u=<user_id> argument.

  -g=             Teamcenter group associated with the -u=<user_id> argument.

  -path=          Existing Teamcenter installation path, if applicable.

  -targetkit=     Path to the Teamcenter media(s) to be deployed.

  -templates=     List of comma separated template name(s) to be deployed. E.g. "foundation,tcae"

  -log=           The path of the log file which would contain results of this execution.

  -h              Display help for this utility.