Cancel
Showing results for 
Search instead for 
Did you mean: 

Export large assembly in TC as JT files

Pioneer
Pioneer

I have a large assembly in TC (created with NX) that I wont to export as a JT assembly so people without TC access can view the assembly JT model with just the free JT viewer. The individual JT files are already created in TC under each part Item revision as a dataset.

 

What's the quickest/easiest way to export this assembly as a JT assembly that can be viewed with JT2go and maintain the assembly structure?

 

Do I have to open the assembly in NX and if so do I need the assembly fully loaded and then use the JT export command? Or is there a quicker way to do this as the JT files already exist?

 

Regards,

Clayton McPherson
TC 10.1, NX 9.0.3.4 MP7
2 REPLIES

Re: Export large assembly in TC as JT files

Siemens Phenom Siemens Phenom
Siemens Phenom

Hi @C_MACCA,

You are referring to the 'Monolithic JT'.

There are couple of topics related to it. Check the suggestions/solutions that may be suitable/useful in your process.

Saving JT files for top level assemblies

Automated export of monolithic JT assembly

 

If the requirement to export JT assembly is not so often then I would suggest to use export JT from managed NX.

 

Re: Export large assembly in TC as JT files

Pioneer
Pioneer

In the end I used the command line utility assy_jt_creator. Seems to have worked ok. Thanks for your help.

Regards,

Clayton McPherson
TC 10.1, NX 9.0.3.4 MP7