Cancel
Showing results for 
Search instead for 
Did you mean: 

FSC Tool to check which node is connected to which FSC Server

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor

Hello,

 

Is there a way to check  which computers are logged to which FSC server, a general overview of all Nodes at once.

 

A manual single-test of all devices is alot of work, especially if there are 100+ Nodes connected to more than one FSC.

 

I didn't find any suitable option by the FSCadmin Tool.

 

Is it possible with Batch maybe?

 

Thanks in Advance

SLR

1 REPLY 1
Highlighted

Re: FSC Tool to check which node is connected to which FSC Server

Solution Partner Esteemed Contributor Solution Partner Esteemed Contributor
Solution Partner Esteemed Contributor
The FSC Admin tool will not do what you are seeking.
From the client side you can try: http://<server>:4544/Ping to validate that an FSC responds.
Or to validate that the client IP is valid for the Subnet/Mask then you can try: http://<server>:4544/mapClientIPtoFSCs?client=10.244.98.110
You might be able to do something in Batch that launches IE to a specific address (like Ping) but that's about it.

I don't know of a direct way to see which FCC's are talking to which FSC's. Another possibility is running 'fccstat -status | find "Assigned"' on each client and then writing it to excel?

Randy Ellsworth, Teamcenter Architect, Applied CAx, LLC
NX 11 | SW 2016 | Creo 4 | TcUA 11.4
Evaluating: AW 3.4