Cancel
Showing results for 
Search instead for 
Did you mean: 

Find something locally search in Teamcenter

Experimenter
Experimenter

Hi,

 

This search that is located near the home tab in the Teamcenter Interface.

 

2015-03-30 12_33_39-My Teamcenter - Teamcenter 9.jpg

 

Is it poissble to get this search not case sensitive?

 

Br,

Jan

 

4 REPLIES

Re: Find something locally search in Teamcenter

Genius
Genius

Yanni,

 

What is the Teamcenter Version, you are using ? On TC 10.1.3; It appears as "filter text" instead of "Search Text", Which is precisely the functionality.

 

Filter Text.JPG

 

Test 1:

Test 1.JPG

 

Test 2:

 

Test 2.JPG

 

Unfortunately, It is Case Sensitive !!

 

Hope this helps.

 

Teamcenter 10.1.7
TC Visualization 10.1.7
NX:11.02 | NX 9.02 | Catia V5 R2012 | AutoCAD 2018 | In-Context Editor |

Re: Find something locally search in Teamcenter

Experimenter
Experimenter

Thank you.

 

It would have been nice if there had been a preference or some kind of setting that would have made the search not Case sensitive..

Re: Find something locally search in Teamcenter

Genius
Genius

Found an option to enable or disable the case sensitivity for searching. Unfortunately not for searching the items locally.

Options.JPG

 

Calls for an ER !!.

Cheers.

Teamcenter 10.1.7
TC Visualization 10.1.7
NX:11.02 | NX 9.02 | Catia V5 R2012 | AutoCAD 2018 | In-Context Editor |

Re: Find something locally search in Teamcenter

Solution Partner Honored Contributor Solution Partner Honored Contributor
Solution Partner Honored Contributor

You might as well get used to case-sensitive searching. The java version problem with Quest Agent while searching help (qagent.jar) in Tc, TcVis and NX that requires special patching appears to be resolved by replacing it with Apache Solr (as seen with NX10 Help). It's also the engine behind Active Workspace. I expect Tc11.2 will leverage Solr. Get to know the future http://lucene.apache.org/solr/features.html

 

Best,

/Randy


Randy Ellsworth, Teamcenter Architect, Applied CAx, LLC
NX 11 | SW 2016 | Creo 4 | TcUA 11.4
Evaluating: AW 3.4