Cancel
Showing results for 
Search instead for 
Did you mean: 

Foundation Database, The current locale, en_IN, is not recognized.

Creator
Creator

I am getting below error while Teamcenter 11.3 Installation. even i changed locale to En_US. 

 

 

Error: 

Foundation Database
The current locale, en_IN, is not recognized. The system must be changed to a known locale in order to install Teamcenter. The following are supported:
en_US, zh_CN, zh_TW, de_DE, es_ES, fr_FR, it_IT, ja_JP, ko_KR, ru_RU, pl_PL, cs_CZ, pt_BR, iw_IL
On Windows systems, go to the Control Panel, Region and Language, Administrative, Change System Locale in order to change the locale.

 

 

2 REPLIES 2

Re: Foundation Database, The current locale, en_IN, is not recognized.

Gears Phenom Gears Phenom
Gears Phenom

Good afternoon, if you are using Windows Server, try additionally install language for display, maybe this will help:

 

https://blog.contabo.com/tutorials/change-display-language-windows-server-2008-r2/

 

 and set all settings, as example:

Advanced2008.jpg

 

 

 

Highlighted

Re: Foundation Database, The current locale, en_IN, is not recognized.

Creator
Creator

@ArthurRM Thank you. Its working now.