Cancel
Showing results for 
Search instead for 
Did you mean: 

Graphics Builder installation

Siemens Pioneer Siemens Pioneer
Siemens Pioneer

Hi all,

 

I have a question for you:

 

is possible to install the graphics builder on a server machine without Nx and use it with a client machine with Nx?

 

I try but when I start the Graphics builder from Classification Admin I have this message:

 

 The graphics builder activation failed

 

The configuration is: Tc10.1 + Nx8.5

 

Can anyone helf me?

 

Thanks

2 REPLIES 2

Re: Graphics Builder installation

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

You can only install the graphics builder on a machine with NX installed, the installation will check if NX is present.

You should be able to install the graphics builder on the client.

Stefan Pendl, Systemmanager CAx, HAIDLMAIR GmbH
Production: NX10.0.3, VERICUT 8.2, FBM, MRL 3.1.7 | TcUA 10.1 MP7 Patch 0 (10.1.7.0) | TcVis 11.4
Development: C (ITK), .NET, Tcl/Tk Testing: NX12.0 | AWC 3.4 Preparing: NX12.0

Employees of the customers, together we are strong ;)
How to Get the Most from Your Signature in the Community
NX Customization - Best Practice Guide

Re: Graphics Builder installation

Experimenter
Experimenter

You have to install NX with three features on server at least:

- UGII

- PVTRANS

- UGMANAGER

 

I have configuration like this and it works. Three features installed on server (server manager) and graphics builder.

And TCCS must be installed on server, too. Just run TCBaseVersion_INSTALLATION_DISTRIBUTIVE\additional_applications\tccs_install\tccsinst.exe. And do not forget install appropriate patch