Cancel
Showing results for 
Search instead for 
Did you mean: 

How to Edit Item Master?

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor

23.PNG

 

 

 How can I edit the Item Master to add more attributes. For Example i have by me:

Benutzerdaten1:

.2:

.3:

Elementkommentar:

Projekt-ID:

Seriennummer:

Vorherige ID:

 

How can I add more stuff here? Its in German by me... But go on and write it in english, its OK.

Thx in advance

 

 

9 REPLIES 9

Re: How to Edit Item Master?

Siemens Phenom Siemens Phenom
Siemens Phenom

Got this from the online help:

 

Siemens-Dokumentation

Forms in the Teamcenter rich client use properties to hold additional information about items. You can add additional properties to custom forms that you create.

  1. Open the Business Objects folder.

  2. Browse to a custom form. All custom forms are children of the Form business object. To search for the business object, you can click the Find button at the top of the view.

  3. Right-click the custom form business object, choose Open, and click the Properties tab in the resulting view.

    The properties of the form appear in a table.

  4. Click the Add button to the right of the Properties table to add properties.

  5. After you add a new property, select the property and ensure that its Enabled and Visible property constants are set to true. This ensures that the property is enabled for use in the user interface.

  6. To save the changes to the data model, choose BMIDESave Data Model, or click the Save Data Model button on the main toolbar.

  7. Deploy your changes to a test server. Choose BMIDEDeploy Template on the menu bar, or select the project and click the Deploy Template button on the main toolbar.

  8. After deployment, test to ensure the property is visible on the form. For example, in the Teamcenter rich client, create an instance of the form by choosing FileNewForm. Open the form instance and verify that the new property is visible on the form.

Re: How to Edit Item Master?

Solution Partner Esteemed Contributor Solution Partner Esteemed Contributor
Solution Partner Esteemed Contributor

A small warning. It's not a good idea to modify the ootb object. A best practice is to create your own Item type and add properties to its Item Master. This may not be an option for you if you've been using the ootb Item type for a while but thought you should be aware.


Randy Ellsworth, Teamcenter Architect, Applied CAx, LLC
NX 11 | SW 2016 | Creo 4 | TcUA 11.4
Evaluating: AW 3.4

Re: How to Edit Item Master?

Genius
Genius

What Randy said x 1000.  Inheritence is your friend.

Re: How to Edit Item Master?

Legend
Legend

Hello SLW,

As nicely told in the other posts, this is done by using the BMIDE . From there I would create a new Business Object, call it BenutzerItem (for example) and add all the properties you need to it. When done, compile and update the template on Teamcenter. The BenutzerItem will be available in the new item creation menu on Teamcenter Graphical User Interface.

 

Es ist das gleiche, wenn auf Deutsch  :)

Re: How to Edit Item Master?

Creator
Creator

We are also looking if this is possible using visual basic once the form has already been created without the need to create any more customised forms.

Highlighted

Re: How to Edit Item Master?

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor

Hello Paul,

 

would you like to edit the original Item Revision Master?

 

I took the advice of Randy, and left it alone. Take a good look at what the user "xtof" wrote.

 

Do you have custom Item type by you?

 

If yes I would recommend you to work with Rendering Stylesheets... You can edit them easily...

 

 

Re: How to Edit Item Master?

Creator
Creator
Would like to edit original item master form as its already there
PROPRIETARY: This e-mail contains proprietary information some or all of which may be legally privileged. It is intended for the recipient only. If an addressing or transmission error has misdirected this e-mail, please notify the author by replying to this e-mail. If you are not the intended recipient you must not use, disclose, distribute, copy, print, or rely on this e-mail.

Re: How to Edit Item Master?

Creator
Creator
Do you need to use BMIDE, C++ or ITK only or can you use Visual Studio for example for the coding?

Re: How to Edit Item Master?

Solution Partner Esteemed Contributor Solution Partner Esteemed Contributor
Solution Partner Esteemed Contributor
You need to use Java and develop it in the Eclipse IDE (see Rich Client Customization Guide). Siemens is free to change this object at anytime and whatever customization you do may break it, be omitted or actually prevent being able to upgrade. It is highly recommended that you create your own object when customizing and leave the OOTB objects alone. You've been warned.

Randy Ellsworth, Teamcenter Architect, Applied CAx, LLC
NX 11 | SW 2016 | Creo 4 | TcUA 11.4
Evaluating: AW 3.4