Cancel
Showing results for 
Search instead for 
Did you mean: 

How to add a custom library to be used by the linker in BMIDE with visual studio

Valued Contributor
Valued Contributor

Hi all,

 

I am doing some test with c++ customization in BMIDE in teamcenter 11.2, I am using an external custom library, my program compile fine but the linker give me an error LNK2019, how can I add to BMIDE the reference to the library, so it can be used in the link process.

 

Thanks for any help, 

 

Regards,

 

Armando Luna

2 REPLIES

Re: How to add a custom library to be used by the linker in BMIDE with visual studio

Siemens Experimenter Siemens Experimenter
Siemens Experimenter

Did you got any solution, PLease share the same.

Re: How to add a custom library to be used by the linker in BMIDE with visual studio

Legend
Legend

You can add extra libraries in the BMIDE to the linker flags in the Build configuration of the project

Then they get automatically added to the makefile (it does so with TC11.3)

 

see also: https://community.plm.automation.siemens.com/t5/Teamcenter-Administrators-Forum/BMIDE-TC12-configura...