Cancel
Showing results for 
Search instead for 
Did you mean: 

How to add an LOV to a Quick Create Dialogue in Teamcenter Systems engineering Rich Client

Siemens Creator Siemens Creator
Siemens Creator

If you see below picture, I am trying to add a LOV to an object_name property which I have defined in BMIDE.

Below is quick Create panel in systems engineering module.

This allows users to create diffrent item types as child item to structure.

 

I dont think, we can control this using stylesheet as I found no stylesheet which is used for QuicKCreate panel dialogue.

Any sugegstion will be appreciated.

 

4.png

1 REPLY 1

Re: How to add an LOV to a Quick Create Dialogue in Teamcenter Systems engineering Rich Client

Solution Partner Esteemed Contributor Solution Partner Esteemed Contributor
Solution Partner Esteemed Contributor
The picture you show is for an application so if it is possible to customize it will require Java and overriding an existing jar for the display along with any user exits written in ITK to support the change in behavior. Both server and client customization would be required to change the application. For sure, it is not a stylesheet change.

Randy Ellsworth, Teamcenter Architect, Applied CAx, LLC
NX 11 | SW 2016 | Creo 4 | TcUA 11.4
Evaluating: AW 3.4