05-08-2017 07:22 AM
Hi there.
Can you please help me how to connecting 2-tier richclient from workstation.
I have teamcenter server and all the things seems to work successful on it, but when i want to connect from a remote workstation with richclient, many errors apear. Ex: "Error allocating Teamcenter user license"
I've used a shared tc_data from server (mapped network drive), and it seems that workstation wants to connect to server.
Ofcourse LMTools is working properly on teamcenter server.
Solved! Go to Solution.
05-08-2017 09:58 AM
NX 11 | SW 2016 | Creo 4 | TcUA 11.4
Evaluating: AW 3.4
05-08-2017 12:45 PM
Thanks for you response.
I've used to disable both the server and client firewalls but the error still appears.
Actually I have 2-tier corporate server + .net manager + web tier for .net (2-tier) and many others, on my server and i want to use a 2-tier richclient (infodba user) from a remote workstation.
Is there any other thing necessary for this topology?
05-08-2017 01:42 PM
NX 11 | SW 2016 | Creo 4 | TcUA 11.4
Evaluating: AW 3.4
05-08-2017 03:07 PM
Thanks again.
My server and client are in the same LAN. I want to install 2-tier richclient due to NX integration.
1. Is there any command or tools to test License manager connection from client?
I want to be assure that it's connection delay problem or any other misconfiguration on tc_data.
2. If i change the structure is it possible to install all the 4-tier components on a single windows server or it needs more than one?
3. As i've seen, the License Manager has a Tcp listening on port 27000, so if the client should have direct connection to License Manager, it may be connection issue again with 4-tier!?
Thanks for you attention
05-08-2017 03:17 PM
NX 11 | SW 2016 | Creo 4 | TcUA 11.4
Evaluating: AW 3.4
05-09-2017 07:36 AM
Thanks
Problem solved with 4-tier topology.