Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

How to disable "Are you sure you want to check-in\out" ?

Genius
Genius

Hello

How to disable "Are you sure you want to check-in\out"  ?

It pops out constantly and makes me do extra mouse clicks.

Teamcenter 11

11 REPLIES 11

Re: How to disable "Are you sure you want to check-in\out" ?

Gears Phenom Gears Phenom
Gears Phenom

Good afternoon, look at the following options in Edit -> Options ...

Confirmation_shown_on_reservation_dialogs = true
Confirm_cancel_checkout_suppressed = true
Confirm_checkin_suppressed = true
Confirm_checkout_suppressed = true

But for me it works a bit strange, correctly work only the first parameter, others do not work. My version of Teamcenter 11.2.3.

Re: How to disable "Are you sure you want to check-in\out" ?

Genius
Genius

Should those 4pcs of parameters be *false* or *true* to disable the pop-up ?

 

Dear NX I'm very very sure and I never ever make no unsure mouse clickings :-)

Unddtitled.jpg

Re: How to disable "Are you sure you want to check-in\out" ?

Gears Phenom Gears Phenom
Gears Phenom

The values for all parameters must be true. But only the first parameter works for me, when you marked check box Do not show confirmation dialog again

Re: How to disable "Are you sure you want to check-in\out" ?

Genius
Genius

Where are those selections ?

Teamcenter 11 (11.4(20171201.00)) 64-bit

Udstitled.jpg

Re: How to disable "Are you sure you want to check-in\out" ?

Gears Phenom Gears Phenom
Gears Phenom

Show conf.png

 

when option Confirmation_shown_on_reservation_dialogs=true

 

Re: How to disable "Are you sure you want to check-in\out" ?

Genius
Genius

Yes. It is in Site-location and at the moment disabled.

I try to make it *true*.

 

123444ed.png

Re: How to disable "Are you sure you want to check-in\out" ?

Gears Phenom Gears Phenom
Gears Phenom

I think you do not need to change the value for Environment:

Specifies whether a preference name can be used (Enabled) as an
environment variable to set the preference value or can not be used (Disabled)
as an environment variable.
You can declare the preference name as an environment variable with an
appropriate value on the TeamCenter server host if the preference definition
contains the Enabled value.
In such cases, the environment variable is considered an instance of a
preference. When the preference definition specifies Environment as
Enabled, a preference search first checks for an environment variable with the
same name as the preference and, if defined, uses that environment variable
value. Otherwise, the normal search pattern for precedence is followed.

Re: How to disable "Are you sure you want to check-in\out" ?

Genius
Genius

So I only change this ?
Confirmation_shown_on_reservation_dialogs = true

and not these ?
Confirm_cancel_checkout_suppressed = true
Confirm_checkin_suppressed = true
Confirm_checkout_suppressed = true

These 3pcs have both User and Site Location:

Un433titled.jpg

Re: How to disable "Are you sure you want to check-in\out" ?

Gears Phenom Gears Phenom
Gears Phenom

With this parameter it works, but it will be necessary to once marked check box "Do not show confirmation dialog again"

Confirmation_shown_on_reservation_dialogs = true

These parameters should be automatically marked check box
"Do not show confirmation dialog again", but they do not work for me

Confirm_cancel_checkout_suppressed = true
Confirm_checkin_suppressed = true
Confirm_checkout_suppressed = true

If you edit a parameter without dba rights, it will create you a user parameter that will only work for you