Cancel
Showing results for 
Search instead for 
Did you mean: 

How to duplicate a unique folder structure

Experimenter
Experimenter

Hello forum

 

I am curious to see if there is any great solutions for how to duplicate a folder in TC and creating a new folder that are unique and not just copying a link.

 

The picture attached to this discussion illustrates my wish for creating a new folder with the same names, but at the same time not just be a link to the first created folder.

 

I have read a bit about ITK program, but could this be the - or part of the solution?

 

This would ease my work to create several folders including a bigger folder structure inside it.

 

My logic dictates me to believe that if you can imagine it, Teamcenter will be able to do so.  

4 REPLIES

Re: How to duplicate a unique folder structure

Phenom
Phenom

I think this can be done with ITK or even with SOA API.

Re: How to duplicate a unique folder structure

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom
You can do this in the Rich Client. File > New > Folder will give you a unique folder and it can be the same name as others in your environment. Copy/Paste will yield a link to an existing folder. So as long as you use New then you will get a unique folder. If you want to build a lot of folders "in mass" then use the MSA tools downloadable from GTAC (tc_extract_msa -report_type=folder) but the folder name has to be unique with this toolset.

Randy Ellsworth, Teamcenter Architect, Applied CAx, LLC
NX 11.0.1.mp01 | SW 2016 | TcUA 11.2.3
Evaluating:AW 3.2

Re: How to duplicate a unique folder structure

Siemens Genius Siemens Genius
Siemens Genius

Hi Randy,

 

Where exactly can this (tc_extract_msa) be downloaded from GTAC?

 

Regards,

Arun

Re: How to duplicate a unique folder structure

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom
Siemens PLM Download Server, Teamcenter and Teamcenter Rapid Start > Product Updates > Tools. Latest file is: Tc10.1_MultiSiteAssist_3.5.3_win64.zip.

Randy Ellsworth, Teamcenter Architect, Applied CAx, LLC
NX 11.0.1.mp01 | SW 2016 | TcUA 11.2.3
Evaluating:AW 3.2