Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

How to read the version and Patch of Teamcenter

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor

Hi everybody,

 

Teamcenter: V10000.1.0.10

Solid Edge: 106.00.13.04

 

The version of teamcenter is 10.1

The Solid Edge version is 6.

 

What can I know more of this? What are the four parts for actually?

 

Thanks in advance!

M

 

3 REPLIES

Re: How to read the version and Patch of Teamcenter

Phenom
Phenom

versionlocal.xml in %TC_ROOT%\install dir contains following info. Here, QRMNumber is the patch number as far as I understand.


    <key id="k_releaseFlag">V</key>
    <key id="k_majorVersion">11000</key>
    <key id="k_minorVersion">2</key>
    <key id="k_QRMnumber">1</key>
    <key id="k_phaseNumber">10_20151116.00</key>
   

Re: How to read the version and Patch of Teamcenter

Siemens Phenom Siemens Phenom
Siemens Phenom

As @xplm2005  shown already

10000.1.0.10

Major Version.Minor Version.QRM Number.Phase or IRM number

 

Major Version: They include major changes to the functionality of the product, enhancements, and usually involve changes to the database.

Minor Version: It designates a maintenance release that doesn't preserve data compatibility with the major enhancement release.

QRM Number: Quick Response Maintenance (QRM). QRMs are intended to release quick fixes to the field.
QRMs are usually reserved for fixes to the product although simple enhancements and minor functionality changes can find their way into them. QRMs preserve two-way data compatibility with all releases that share the same major/minor release.

IRM Number: In the context of a major release, this field identifies the phase number and is used to identify beta versions. In the context of a QRM release, this field identifies an Immediate Response Maintenance Release (IRM). If absolutely necessary, an IRM can be shipped to a customer to address a critical problem. IRMs preserve two-way data compatibility with all releases that share the same major/minor release.

Regards,
Ganesh

Re: How to read the version and Patch of Teamcenter

Experimenter
Experimenter

 

  • Recommended System Configuration:

  • 64-bit (x64) processor
  • Windows XP Professional Service Pack 2
  • At least 4 GB RAM
  • True Color (32-bit) or 16 million colors (24-bit)
  • Screen resolution set to 1280 x 1024
  • Disk space: The unmanaged data will be copied to the local drive (SEEC cache). The amount of free space must be greater than the amount of unmanaged data to be imported into Teamcenter.

 

https://gpahub.net/college-gpa-calculator