Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

How to replace linked body when importing into teamcenter

Pioneer
Pioneer

2018-01-02_10h56_47.pngWe are now working with team center and I would like to import a model .prt (nx native) file that have linked bodies that are also NX native but were not created through teamcenter... SO I would either like to only import the master model without the linked bodies ... or change the linked bodies from other models that are already imported into teamcenter.. please see attaached image ..in the red rectangle are the files I would like to cancel importing or swap