Cancel
Showing results for 
Search instead for 
Did you mean: 

How to set status on multiple targets based on property of attached target objects?

Experimenter
Experimenter

I have multiple target objects of same type in a workflow. Can I set different statuses on objects based on the property value.

 

Example: 10 Document objects are attached as targets to a workflow task. Document object has an attribute "Size" which can have Value "Small" or "Big" (LOV). I want to set a status of "Approved" on all the targets with value Size=Small and Rejected status on Size=Big. Is this possible using OOTB handlers?

 

Thanks

John

2 REPLIES 2

Re: How to set status on multiple targets based on property of attached target objects?

Siemens Phenom Siemens Phenom
Siemens Phenom

Hi,

Have a look at the documentation of the EPM-set-condition action handler. You can build a query and move the objects that do not meet the condition from workflow target to reference. Then branch your workflow and set the status in the branches of your workflow.

HTH,

xtof

Highlighted

Re: How to set status on multiple targets based on property of attached target objects?

Valued Contributor
Valued Contributor

Hi John,

 

Better option is to use sub workflow for each document, EPM-set-condition (query which controls the decision) on the Sub workflow and upon result the accurate status is been set.

 

Regards,

Chene