Cancel
Showing results for 
Search instead for 
Did you mean: 

How to work with IRDC in BMIDE

Experimenter
Experimenter

Hi,

 

I am unable to understand IRDC Concept and how it is working. Kindly help me.

 

Thanks,

Sandhiya. 

1 REPLY 1

Re: How to work with IRDC in BMIDE

Experimenter
Experimenter

We use IRDC since upgrade from TC 8.3 to 11.2. Siemens has configured it for us, so I do not have a lot of details for you. As far as I see you need two components:

1. An IRDC object with the "template". This is de dataset which will be copied from.

2. A rule in BMIDE which tells which template is used when creating which item.

 

Make sure that the IRDC object is released with a status with the text "release" in it.

I am sure the documentation tells you a lot more. I hope this helps you a bit.