Cancel
Showing results for 
Search instead for 
Did you mean: 

How users collaborate in TCRS when they are located accross countries?

Solution Partner Pioneer Solution Partner Pioneer
Solution Partner Pioneer

We have one possible customer and they want TCRS to be accessed by their other engineer in other counties. These engineers are part of the design and approval processes. They want to have a single platform which can connect them to perform their tasks easily.

 

Any idea on how can this be done?

 

1 REPLY

Re: How users collaborate in TCRS when they are located accross countries?

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom
If the Engineer is not creating (authoring) data then they can access Teamcenter through the web client to perform review/approval of workflow tasks. If the Engineer is authoring then it may be appropriate to set up a Store and Forward volume at their location. It may make financial sense to stand up a remote FSC for a single user so another option is to put a workstation in the server room at corporate and let them login into via VPN to launch and participate in Teamcenter.

Randy Ellsworth, Teamcenter Architect, Applied CAx, LLC
NX 11 | SW 2016 | Creo 4 | TcUA 11.4
Evaluating: AW 3.4