Cancel
Showing results for 
Search instead for 
Did you mean: 

IMAN_reference block cut and paste

Pioneer
Pioneer

Hi,

 

when have Items even those have status we're available to cut and paste to add or IMAN_reference inside. How could I block the permissions to cut and paste IMAN_reference when the parent Item has status?

 

Thanks in advance

2 REPLIES 2

Re: IMAN_reference block cut and paste

Valued Contributor
Valued Contributor

Ability to paste or cut a secondary object from its primary is controlled using the "attachability" and "detachability" values defined as a part of the GRM rule for the given primary, secondary and the relation type in BMIDE.

 

If the "attachability" is set to "Unrestricted", no matter the status of the primary users will be able to paste objects for a given relation. If you change the value to "WriteAccessReq", then the users have to have write access on the primary object to be able to paste objects under it.

Re: IMAN_reference block cut and paste

Pioneer
Pioneer

Question solved, thanks I changed it and it worked.