Cancel
Showing results for 
Search instead for 
Did you mean: 

Import drawing from Native to TC

Solution Partner Genius Solution Partner Genius
Solution Partner Genius

Hi, 

I need to import the drawing of an assembly (Master Model method) from OS into TC (as a specification of the Item Revision)

I can easily do it with revision 0/0, in working.

But I cannot do when the Item Rev has in TC has increased (see image below: the drawing was mad with rev 0/0 and must be imported into rev 1/0). I think it is something related to the 'Name ad Attribute' options but I tried different combination with no success.

Thank you for help

Image 1

 

Image 2image 1.jpg

 

image 2.jpg

 

 

 

 

 

3 REPLIES 3

Re: Import drawing from Native to TC

Siemens Esteemed Contributor Siemens Esteemed Contributor
Siemens Esteemed Contributor

Hi @Laurus,

 

See if the following video helps.  I captured importing a drawing to an existing item, where the drawings item ID already existed (previously imported) in Teamcenter, and then importing a drawing to an existing item ID whose master item ID is different that the original native filename.  The important step to note is when I change the "Relation Type" from "master" to "specification" (at 00:35 and 01:33) for the drawing being imported.

 

(view in My Videos)

 

Hope that helps.

Regards, Ben

Ben Broad | PLM Enthusiast | Siemens GCSS

NX (v17 - 1876) | Teamcenter (9 - 12)
Value Based Licensing | Adaptive UI | BETA Registration

Re: Import drawing from Native to TC

Solution Partner Genius Solution Partner Genius
Solution Partner Genius

Thank you very much Ben,

this is what I needed. One question: which parameter did you choose to import the Master Model (Use existing?)

tc import.jpg

Re: Import drawing from Native to TC

Siemens Esteemed Contributor Siemens Esteemed Contributor
Siemens Esteemed Contributor

@Laurus wrote:

Thank you very much Ben,

this is what I needed. One question: which parameter did you choose to import the Master Model (Use existing?)

 


Yes.

 

Regards, Ben

Ben Broad | PLM Enthusiast | Siemens GCSS

NX (v17 - 1876) | Teamcenter (9 - 12)
Value Based Licensing | Adaptive UI | BETA Registration