Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

Installing NX templates in teamcenter

Genius
Genius

Hello everyone

 

I have a problem with NX template

I open NX than I got worning

"I don't have template!"

 

SO,how I solve this problem?

I need to know the installing NX template step

where I need to try this? Server or client?

Best Regards
David
Teamcenter 11.4,Active Workspace 3.4
Solid Edge ST10
6 REPLIES 6

Re: Installing NX templates in teamcenter

Siemens Honored Contributor Siemens Honored Contributor
Siemens Honored Contributor

You need to install templates on the server:  Installing File New Templates

 

Regards, Ben

Re: Installing NX templates in teamcenter

Genius
Genius

Hello BenBroad

 

How should I know my

 

UGII_UGMGR_COMMUNICATIO

UGII_UGMGR_HTTP_URL

 

location?

 

Can you screenshot for me?

 

thank you!

Best Regards
David
Teamcenter 11.4,Active Workspace 3.4
Solid Edge ST10

Re: Installing NX templates in teamcenter

Siemens Honored Contributor Siemens Honored Contributor
Siemens Honored Contributor
It sounds like you already have NX Integration installed as you mentioned that you started NX and got a warning that you don't have templates. Are you using 2-tier or 4-tier?
The variables you mention above are for 4-tier. From an NX Integration session select "Help > Log File" and search for "tier". This should tell you which tier your using. If it says 4-tier then search for the variables UGII_UGMGR_COMMUNICATION and UGII_UGMGR_HTTP_URL to find their values so you know what to use in the command window.
If it says 2-tier then you need to set TC_ROOT and TC_DATA in the command window to install the templates.

Regards, Ben

Re: Installing NX templates in teamcenter

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

In addition to use the utilities, you can always use File => Import assembly into Teamcenter directly from a managed NX session, which avoids messing around with variables and scripts ;)

Stefan Pendl, Systemmanager CAx, HAIDLMAIR GmbH
Production: NX10.0.3, VERICUT 8.2, FBM, MRL 3.1.7 | TcUA 10.1 MP7 Patch 0 (10.1.7.0) | TcVis 11.4
Development: C (ITK), .NET, Tcl/Tk Testing: NX12.0 | AWC 3.4 Preparing: NX12.0

Employees of the customers, together we are strong ;)
How to Get the Most from Your Signature in the Community
NX Customization - Best Practice Guide

Re: Installing NX templates in teamcenter

Genius
Genius

Hello BanBroad

 

I use 2-tier to setup , but it still wrong!
15_x_15_10-07-56.png

 

what did I miss?

 

I already build environment variable TC_ROOT and TC_DATA

 

Best Regards
David
Teamcenter 11.4,Active Workspace 3.4
Solid Edge ST10

Re: Installing NX templates in teamcenter

Genius
Genius

I found that  java can't identify file's name with space(EX c:\program file

 

so,no matter what I try it still not working

 

I reinstall NX and command again,it works!!!

Best Regards
David
Teamcenter 11.4,Active Workspace 3.4
Solid Edge ST10