Cancel
Showing results for 
Search instead for 
Did you mean: 

Installing Teamcenter 12 RAC and NX12 next to TC8 RAC and NX8

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor

Hello!

 

I installed NX12 and TC12-client on a computer that has NX8 and TC8-client. Teamcenter 8 and 12 works fine but when starting NX8 from Teamcenter 8 It gives an error (Attached).

 

I added the following command to TC12 portal.bat:

reg add HKCR\ugmportalfile\Shell\Open\command /d "%TPR%\start_nxmanager.bat" /f

 

I also set if else commands to start_nxmanager.bat scripts where if TPR is TC12ROOT\portal set UGII_BASE_DIR to NX12_ROOT and else if it is TC8ROOT\portal set UGII_BASE_DIR to NX8_ROOT.

 

What else should I do? Is NX8 old enough that it uses different registry keys?

1 REPLY 1
Highlighted

Re: Installing Teamcenter 12 RAC and NX12 next to TC8 RAC and NX8

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor
Well.. I also added "reg add HKCR\ugmportalfile\Shell\Open\command /d "%TPR%\start_nxmanager.bat" /f" to the TC8 portal bat and it fixed the problem.