Cancel
Showing results for 
Search instead for 
Did you mean: 

Integration between Teamcenter 10 and NX 10

Pioneer
Pioneer

Hello 

I have been trying to find information regarding how to integrate NX and Teamcenter and I have not find anything. I already have Teamcenter 10 4-tier Rich Client and NX 10 installed but I can no find how to connect them. If someone can provide me with the information of how I can integrate them and which packege is needed be to installed in order to have them integrated I would appreciete it. 

 

Thanks

cabd87

19 REPLIES

Re: Integration between Teamcenter 10 and NX 10

Siemens Phenom Siemens Phenom
Siemens Phenom

Hi,

You have to install the Teamcenter integration for NX with tem. check the boxes as shown on the screenshot.
2016-09-13 12_23_12-Teamcenter 11.png

To be able to start NX from Teamcenter RAC check the following preference:

 

 

Re: Integration between Teamcenter 10 and NX 10

Pioneer
Pioneer

First all thaks xtof

 

I already have installed the Teamcenter Integration for NX as can be seen in the screenshot of my configuration but I am still no able to connect them. I dont know waht else can be. When I tried to run NX 10 from RAC it said "Failed to start application UGManager".  Any idea what else I can tried or If I need to add any other feature in the TEM????

 

Screenshot.jpg

 

 

Re: Integration between Teamcenter 10 and NX 10

Siemens Phenom Siemens Phenom
Siemens Phenom
In the portal directory of Teamcenter there should be a file called: start_nxmanager.bat. Do you have it?
Look in the registry for ugmportalfile. The command should point to the start_nxmanager.bat.

Re: Integration between Teamcenter 10 and NX 10

Pioneer
Pioneer

Hi I could find the file ... What should I do?

file.png

Re: Integration between Teamcenter 10 and NX 10

Esteemed Contributor
Esteemed Contributor

If the file is there, it should be OK.

Have you installed NX with the typical installation or with a custom one?

Make sure that the NX-Manager module is installed, might also be call UG-Manager, haven't used custom installation for a while.

Stefan Pendl, Systemmanager CAx, HAIDLMAIR GmbH
Production: NX10.0.3, VERICUT 8.0, FBM, MRL 3.1.4 | TcUA 10.1 MP7 Patch 0 (10.1.7.0) | TcVis 10.1
Development: VB.NET, Tcl/Tk    Testing: NX12.0

How to Get the Most from Your Signature in the Community

Re: Integration between Teamcenter 10 and NX 10

Pioneer
Pioneer

I installed with the typical installation and the UG Manager is installed as well since I can find a folder full of files in the NX directory. Should I configure something in teamcenter to be able to run NX...coz I can no find any reason...

Here is the message I got when I tried to run it from teamcenter.

 

Capture1.PNG

Re: Integration between Teamcenter 10 and NX 10

Siemens Phenom Siemens Phenom
Siemens Phenom
This is from the FAQ of Siemens GTAC:

To test ugs_router

From Windows command prompt:
4 Tier
set UGII_UGMGR_COMMUNICATION=http
set UGII_UGMGR_HTTP_URL=http://hostnameSmiley Tongueort/tc
%UGII_ROOT_DIR%\ugs_router -ugm

2 Tier
%UGII_ROOT_DIR%\ugs_router -ugm

NX/Manager started and log on OK.

Test MIME type ugmportal

cd %PORTAL_ROOT%
runner -mime=application/ugmportal

No pop-up! Mime type issue. Missing entry

Search for registry keys:

1/. HKEY_CLASSES_ROOT\ugmportalfile\Shell\Open\command
%PORTAL_ROOT%\start_nxmanger.bat

2/. HKEY_LOCAL_MACHINE\SOFTWARE\Classess\ugmportal

Found that NX Manager for Rich Client Feature was not installed. Once installed
NX launched without issue. Ensure these Registry entries are set and correct if
this error is seen.

Re: Integration between Teamcenter 10 and NX 10

Pioneer
Pioneer

Hello

Once I oppened Command Prompt, this messange came up...

Capture3.PNG

 

it says something to you?

Re: Integration between Teamcenter 10 and NX 10

Siemens Phenom Siemens Phenom
Siemens Phenom
again from GTAC FAQ:

Solution
This variable is set when the Microsoft development libraries are installed.
It can be ignored.