Cancel
Showing results for 
Search instead for 
Did you mean: 

Integration of NX UDF Library with Teamcenter

Experimenter
Experimenter

Hello All,

 

I want intigrate User defined Library created Locay with my Teamcenter 10.0.

How can i do that ??  Please Help me out.

I have done some changes in Utilities>Customer Defaults and able to accese UDF library when using NX localy but not when use through Teamcenter.

For more clarification please refer images.

 

Thanks

Manoj

1 REPLY 1

Re: Integration of NX UDF Library with Teamcenter

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

There is a setting in ugii_env.dat that allows usage of the native UDF library in a managed NX session.

 

BTW, cross-posting just confuses, since the discussion is divided into two or more threads and therefore it is not good practice to do so in a forum.

Stefan Pendl, Systemmanager CAx, HAIDLMAIR GmbH
Production: NX10.0.3, VERICUT 8.2, FBM, MRL 3.1.7 | TcUA 10.1 MP7 Patch 0 (10.1.7.0) | TcVis 11.4
Development: C (ITK), .NET, Tcl/Tk Testing: NX12.0 | AWC 3.4 Preparing: NX12.0

Employees of the customers, together we are strong ;)
How to Get the Most from Your Signature in the Community
NX Customization - Best Practice Guide