Cancel
Showing results for 
Search instead for 
Did you mean: 

Is it possible to log in TC from outside local area network?

Genius
Genius

I would like to know if that is possible and if it is easy to do. It would be good if connecting to TC is possible but I would like to connect also to NX manager (my NX license server is installed in my laptop). Thanks

6 REPLIES 6

Re: Is it possible to log in TC from outside local area network?

Siemens Phenom Siemens Phenom
Siemens Phenom

It is not possible to access TC from outside network unless you are connected to the company network using VPN.

 

 

Re: Is it possible to log in TC from outside local area network?

Legend
Legend

If the web port is open you should be able to access Teamcenter from a web browser by using its URL. (As far as Teamcenter was configured to give service over the web). Just append /tc/webclient to the server's address.

https://[server]/tc/webclient

 

 

Re: Is it possible to log in TC from outside local area network?

Siemens Phenom Siemens Phenom
Siemens Phenom

@PLMFan wrote:

If the web port is open you should be able to access Teamcenter from a web browser by using its URL. (As far as Teamcenter was configured to give service over the web). Just append /tc/webclient to the server's address.

https://[server]/tc/webclient

 

 


That would be thin client, Right...?

Re: Is it possible to log in TC from outside local area network?

Legend
Legend

That is right :) But also the Rich one, it uses the same ports.

Highlighted

Re: Is it possible to log in TC from outside local area network?

Solution Partner Esteemed Contributor Solution Partner Esteemed Contributor
Solution Partner Esteemed Contributor
Danger: exposing ports defeats you network security. Best practice in this case is to setup a Teamcenter instance outside the DMZ then use multisite with production Teamcenter (inside the DMZ) to export/import over only the data you want exposed to the other Teamcenter (outside the DMZ). The Teamcenter outside the DMZ is at risk while your production Teamcenter remains inside the DMZ and is safe. It's a lot of work to maintain this configuration and is rarely worth the effort. I don't know of any company using this configuration but it is possible.

Randy Ellsworth, Teamcenter Architect, Applied CAx, LLC
NX 11 | SW 2016 | Creo 4 | TcUA 11.4
Evaluating: AW 3.4

Re: Is it possible to log in TC from outside local area network?

Legend
Legend

Randy is right, be like Randy.

In general, publishing military or industry data even through secured ports is really very risky. Anyway, in Mad-Max scenarios communicating with Teamcenter using well known ports is perfectly possible and I deserve many Kudos for my answer.