Cancel
Showing results for 
Search instead for 
Did you mean: 

Limit on number of UGPART datasets

Experimenter
Experimenter

First time poster.

 

Is there a limit in Teamcenter on the number of UGPART/Drawing Sheets that an item revision can have?  We heard a rumor that Siemens has put a limit on the number of UGPART datasets that Teamcenter can support.  We have a number of item revisions with as many as 150 UGPART/Drawing Sheets.  Just looking for verification of that and, if it's true, what is that limit?

 

Thank you for your assistance.

 

Dave Barnett

2 REPLIES

Re: Limit on number of UGPART datasets

Pioneer
Pioneer

Dave,

as I see there is not limitation OOTB (TC10.1) within the datamodel how many UGPART dataset can be attached to an ItemRevision in IMAN_manifestation or IMAN_specification relation which are the usual ones for UGPART.

 

 

Thomas Zwatz, CADadmin, PÖTTINGER Landtechnik GmbH
Production: NX11.0.2.7 MP4 + TC10.1.7.1
Testing: NX11.0.2.7 MP4 + TC10.1.7.1
Development: C#

Re: Limit on number of UGPART datasets

Legend
Legend
See preference AE_dataset_default_keep_limit