Cancel
Showing results for 
Search instead for 
Did you mean: 

List deprecated functions of TC8

Builder
Builder

I have one customized executable(dll) file.Is there any way to extract functions which are deprecated in TC8?

4 REPLIES

Re: List deprecated functions of TC8

Hello SwamyRangu,

What do you actually mean by 'extract'? "List the deprecated functions" or "completely remove the functions from the dll" instead? 

 

Re: List deprecated functions of TC8

Builder
Builder

@Ramon_Talavera,

 

For example, I have one custom dll file which is developed on TC 8. Now,i would like to upgrade that by recompiling. So i need to list out all deprecated functions of tc8 w.r.t tc 10/tc 11.

Re: List deprecated functions of TC8

Not easy, but feasible. The deprecated methods are marked in the documentation. Perform a search over the API documentation and collect all methods marked as 'deprecated', once done, search into the code for functions that match the obtained list, this could be automatically done (cross search the list with the dll's code looking for matches). In JAVA that could be 'easily' done by adding -deprecated parameter during compilation. In C++ everything is a little bit harder, as usually, as solving controversies with its language fans.

 

(FYI: The "deprecated functions" list is not an enormous one).

Re: List deprecated functions of TC8

Builder
Builder

@Ramon_Talavera,

 

By referring docs, we can identify. It is time consuming..Smiley Happy