Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

Manufacturing Process Planner - Custom Report

Experimenter
Experimenter

Is there any way to gerenate a report where all the parent items are displayed in the same row starting from a particular level?

 

Normally the structure looks like this. 

Level 0: Item A

Level 1: Item B

Level 2: Item C

 

Level 0: Item X

Level 1: Item Y

Level 2: Item Z

----------------------------------------------------------

I want to generate a report similar to the one below. The parent of the previous column will have to be displayed in the next column.

 

1. Item C        Item B         Item A

2. Item Z        Item Y         Item X

 

Thanks,

Ganesh G.

2 REPLIES 2

Re: Manufacturing Process Planner - Custom Report

Solution Partner Esteemed Contributor Solution Partner Esteemed Contributor
Solution Partner Esteemed Contributor

I've heard of a two column report (flattened BOM):

  • A and B
  • B and C
  • X and Y
  • Y and Z

But not a three column report? You might need custom code for that kind of formatting.


Randy Ellsworth, Teamcenter Architect, Applied CAx, LLC
NX 11 | SW 2016 | Creo 4 | TcUA 11.4
Evaluating: AW 3.4

Re: Manufacturing Process Planner - Custom Report

Experimenter
Experimenter

Thanks for the reply. It is not just a three column report. The columns may increare based on the level I need. I am also looking into the scripts/ codes. Thanks again.