Cancel
Showing results for 
Search instead for 
Did you mean: 

Mapping custom Inventor properties to TC attributes

Creator
Creator

Hi,

 

We are trying to map custom Inventor properties to Teamcenter attributes through the Attribute mapping as given in the documentation. But we were not able to reflect the properties that are being added even in the Inventor to Teamcenter.

{ Dataset type="AIPart"
{ 
 Item type="GNFabPart"
       
		"User Defined Properties_Hardening" : ItemRevision.gnhardening /master=both
		"User Defined Properties_Mass" : ItemRevision.gnmass /master=cad
    } 
}

The above is the snippet of the code, here Hardening and Mass are custom created properties with respect to the part file

 

Regards

 

TC12, Inventor 2018

@Jamie_Griffis 

@RandyEllsworth 

2 REPLIES 2

Re: Mapping custom Inventor properties to TC attributes

Solution Partner Esteemed Contributor Solution Partner Esteemed Contributor
Solution Partner Esteemed Contributor
First, check your spelling. Your Item and properties must have the real values that match case-wise.
Second, allow for a null value with "/allow_null_value"
Third, add a description with /description="Hardening" similar to a tool tip
Forth, the first term will be the unique name of the property created
Fifth, when including properties from the Item then /master must be iman.

Fab Hardening : ItemRevision.GNHARDENING /master=both /allow_null_value /description="Hardening"

Randy Ellsworth, Teamcenter Architect, Applied CAx, LLC
NX 11 | SW 2016 | Creo 4 | TcUA 11.4
Evaluating: AW 3.4

Re: Mapping custom Inventor properties to TC attributes

Creator
Creator

Hi @RandyEllsworth ,

 

It has been sorted out, after importing the mapping .txt file, the server was refreshed and it solved the problem, no errors in the syntax as such. Peace.

 

Regards