Cancel
Showing results for 
Search instead for 
Did you mean: 

NX 10 and Teamcenter

Valued Contributor
Valued Contributor

I am having some issues with using NX 10 through Teamcenter.

 

when I edit the arangements it changes all the arrangements 

 

When I try to create a new part, the XRX model and drawing templates to not show up. 

 

 

When I use NX through my desktop I have none if these issues. Does anyone know wth is going on?

3 REPLIES 3

Re: NX 10 and Teamcenter

Siemens Esteemed Contributor Siemens Esteemed Contributor
Siemens Esteemed Contributor
The behavior should not be any different between native or managed NX.
How are you editing an arrangement such that all arrangements are changed? Are you moving a component? Is that component independently positioned or "same position in all"?

If templates are not displayed when creating a new part in managed NX, then it's quite possible that NX templates have not been imported into the database.

Regards, Ben
Highlighted

Re: NX 10 and Teamcenter

Valued Contributor
Valued Contributor
How would I go about importing templates into the database?

Re: NX 10 and Teamcenter

Siemens Esteemed Contributor Siemens Esteemed Contributor
Siemens Esteemed Contributor