Cancel
Showing results for 
Search instead for 
Did you mean: 

NX Assembly Teamcenter Incomplete Transfer

Experimenter
Experimenter

Hi,

 

I am using NX 8.0.3.4 and Teamcetner 8 (8.3.3.1)

 

While transferring assemblies from remote to local, though "Inlcude Entire BOM" selected it seems some components are missed after transfer was over and  I re-do the components that are not transferred; For example i noticed that when a component is set as "Part is reference only" inside the assembly, which excludes from the transfer though all References selected in Relationship options in Remote Export.

 

Could anyone please suggest why "Inlcude Entire BOM" does not work all times, what type of parts cause or reasons behind this kind of incomplete transfer..?

 

Please find attached for reference.

 

Thanks for helping,

 

Regards,

Dilli

 

2 REPLIES

Re: NX Assembly Teamcenter Incomplete Transfer

Creator
Creator

Please check on this following:

1) Access on the Failed part.

2) Sometimes if part is checked out then it wont happen.

 

Let me know.

Re: NX Assembly Teamcenter Incomplete Transfer

Experimenter
Experimenter

Hi,

 

I am trying to transfer without Ownership, to use it on another assembly,

so

1. I need to check with the failed part, however i do not have access on that, it is read-only and owned by remote user.

2. While transfering without ownership (where part check-out not required) also the error comes..

 

Thanks for your reply..