Cancel
Showing results for 
Search instead for 
Did you mean: 

NX INTEGRATION ISSUE

Pioneer
Pioneer

Hello

I am not able to open NX 10 from TC 11. I have attached the error which pops when I try to open.Capture.PNG 

11 REPLIES

Re: NX INTEGRATION ISSUE

Siemens Phenom Siemens Phenom
Siemens Phenom

looks like no entries in the registry.

Is NX feature installed in RAC?

Open cmd in portal dir and execute runner -mime=application/ugmportal. Another shell should pop-up. If nothing happens you have to add the installation or manually some entries to registry.

xtof

Re: NX INTEGRATION ISSUE

Solution Partner Honored Contributor Solution Partner Honored Contributor
Solution Partner Honored Contributor

Best practice is to install NX first then TC. There should be a PORTAL_ROOT\start_nxmanager.bat script if the NX integration is installed. If you had a previous version of NX installed then the registry setting could still be pointing to the old location. Search for start_nxmanager.bat in the registry and validate the location is correct.


Randy Ellsworth, Teamcenter Architect, Applied CAx, LLC
NX 11 | SW 2016 | Creo 4 | TcUA 11.4
Evaluating: AW 3.4

Re: NX INTEGRATION ISSUE

Pioneer
Pioneer
Right. I have no entries in registry. my start_ugmanager.bat file is missing and I also have an older version of NX8.5. should I uninstall that. Would that help.?

Re: NX INTEGRATION ISSUE

Pioneer
Pioneer
Well regardless of my previous reply. I have 2 start_nxmanager.bat files. I have attached an image for both the location files. the 1st one under TC files and other under program files. Do I need both the .bat file?

Re: NX INTEGRATION ISSUE

Solution Partner Honored Contributor Solution Partner Honored Contributor
Solution Partner Honored Contributor

No image?


Randy Ellsworth, Teamcenter Architect, Applied CAx, LLC
NX 11 | SW 2016 | Creo 4 | TcUA 11.4
Evaluating: AW 3.4

Re: NX INTEGRATION ISSUE

Siemens Valued Contributor Siemens Valued Contributor
Siemens Valued Contributor
Hi

you must have 2 bat files "nxmanager_portal" & "start_nxmanager" under "C:\Program Files\Siemens\Teamcenter11\portal" if you have installed "Teamcenter Integration for NX". If not then please install the same using TEM. You can find TEM at "C:\Program Files\Siemens\Teamcenter11\install".  Double click the TEM and  you can find "Teamcenter Integration for NX" in under "Extensions". I have attached a screen shot.

Thanks

Anshu

Re: NX INTEGRATION ISSUE

Pioneer
Pioneer

I have both the .bat files under the location of C: and also I have NX10 integration for TC installed but its still giving me that error. I have no clue.

Re: NX INTEGRATION ISSUE

Pioneer
Pioneer

Capture1.PNG

Re: NX INTEGRATION ISSUE

Siemens Phenom Siemens Phenom
Siemens Phenom

you really have to make sure that the registry entries are there. 

Do you see start_nxmanager.bat here  [HKEY_LOCAL_MACHINE\SOFTWARE\Classes\ugmportalfile\Shell\Open\Command] in the registry?