Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

New Dataset file types

Creator
Creator

Hi All,

 

Just a quick question regarding the time it takes to enable new file extensions in Teamcenter.

I'm a end user with no admin access so just curious as to the time burden a request for a new dataset eg .docx and .docm being added.

 

Thanks, and looking forward to your responses

2 REPLIES 2

Re: New Dataset file types

Experimenter
Experimenter

Hello Ben_849 ,

It depends on the type of dataset being added , if it's a normal file extension like .docx or .xlsx it hardly takes a minute or so.  There are numerous types of datasets predefined in Teamcenter. However, your site may need to add more types to be able to manage your site’s specific application data files and the viewing/editing software applications associated with these files.

 

so , just selecting the tool to view and tool to edit the dataset is all u need and then ofcourse time required to deploy the template.

Re: New Dataset file types

Creator
Creator
Thanks for the reply
Confirmed everything I expected
Have a great weekend!!