Cancel
Showing results for 
Search instead for 
Did you mean: 

Not allowing Save and Check-in if there is any error in Form

Pioneer
Pioneer

In TC10, after clicking on Save and Check-in the Check-in window comes even if there is an error(i.e. Required Field is blank).

Is there any way (including customization)to prevent that if there is an error. In short, user should not be allowed to Check-in the form if there is an error while saving it.

Check-IN.jpg

 

 

1 REPLY

Re: Not allowing Save and Check-in if there is any error in Form

Solution Partner Legend Solution Partner Legend
Solution Partner Legend
You can set the property constant "required" for the property to TRUE in BMIDE. With this setting the save button remains deactivated untill the required fields are empty.