Cancel
Showing results for 
Search instead for 
Did you mean: 

Override existing Menu Items in Teamcenter 9.1

Experimenter
Experimenter

Hello Experts,

 

How to override an existing Menu item in Teamcenter 9.1 using plugin.xml.

 

For example: I need to disable "Project" menu under Tools for all ItemRevisions.

 

Thanks in advance.

 

Regards,

Gopal

2 REPLIES 2

Re: Override existing Menu Items in Teamcenter 9.1

Genius
Genius

You can use the command suppression application and specify, which groups to not have these commands, Once you supress these will be  hidden from the Create / Revise panels also.

 

Hope this helps !

Cheers.

Teamcenter 10.1.7
TC Visualization 10.1.7
NX:11.02 | NX 9.02 | Catia V5 R2012 | AutoCAD 2018 | In-Context Editor |

Re: Override existing Menu Items in Teamcenter 9.1

Experimenter
Experimenter

Hi,

 

Thanks for the quick response. However, with Command Suppresion can we suppress the menu item for all groups (i.e for all Tc Users when an Item Revision is selected the Project -> Assign menu should be diabled)

 

Thanks,

Gopal