Cancel
Showing results for 
Search instead for 
Did you mean: 

Re: Upgrade TCVis 9 to TCVis 11.3: X_T File is not visible

Experimenter
Experimenter

Hello,

 

Since 3 Years i'm using TC for showing Parasolids (neccesary to make screenshots for my operating instructions).

4 ago i made an update from TC 9 to TC 11.3.

 

The Problem: X_T-Files i got from Engineering are no longer Visible in TC 11.3

In TC 9 there are all working.

 

In the Attachment the problem is shown.

The little Pre-View on the left Side is Working.

 

Need some help.

Please

9 REPLIES

Re: Upgrade TC 9 to TC 11.3: X_T Fileis not visible

Solution Partner Honored Contributor Solution Partner Honored Contributor
Solution Partner Honored Contributor
The image shows a parasolid in Teamcenter Visualization? What version of Parasolid files are you trying to view in TcVis 11.3? With NX, you can find the version in the syslog but I don't know where to find that in TcVis.

NX 8.0

*** Enabling SMP using 4 threads on 4 processors ***
Parasolid version 24.0 build 143 on 19:45:2 12-5-2011

NX 8.5

*** Enabling SMP using 4 threads on 8 processors ***
Parasolid version 25.0 build 248 on 19:45:3 21-6-2013

NX 9

*** Enabling SMP using 4 threads on 8 processors ***
Parasolid version 26.1 build 231 on 19:45:2 17-7-2014

NX 10:

*** Enabling SMP using 4 threads on 8 processors ***
Parasolid version 27.0 build 178 on 19:45:03 16-08-2014

Randy Ellsworth, Teamcenter Architect, Applied CAx, LLC
NX 11 | SW 2016 | Creo 4 | TcUA 11.4
Evaluating: AW 3.4

Re: Upgrade TC 9 to TC 11.3: X_T Fileis not visible

Experimenter
Experimenter

Sorry but i have no NX on my Desktop PC.

 

I used TC 9 for showing Parasolids in Format "*.vf" and "x_t"

an one other one.

 

It worked perfectly to show components, fade out parts  and making screenshots für the manuals

(i'm technical writer)

Re: Upgrade TC 9 to TC 11.3: X_T Fileis not visible

Solution Partner Honored Contributor Solution Partner Honored Contributor
Solution Partner Honored Contributor
You're using Teamcenter Visualization and not Teamcenter? Those are separate applications and I just want to be clear on which? I'm not an expert in Teamcenter Visualization if that's what you're using so someone else will need to step in to answer. There is likely a setting in TcVis to enable viewing older parasolid versions so knowing which version of a parasolids file (x_t) will be important to know.

Randy Ellsworth, Teamcenter Architect, Applied CAx, LLC
NX 11 | SW 2016 | Creo 4 | TcUA 11.4
Evaluating: AW 3.4

Re: Upgrade TCVis 9 to TCVis 11.3: X_T File is not visible

Experimenter
Experimenter

Thank you Randy.

 

I use TCVis, thats correct. Sorry

Actually i can't see the version of my X_T-File in File Details.

So next week i'll ask the engineer what X_T Version he created for me.

 

 

 

Re: Upgrade TCVis 9 to TCVis 11.3: X_T File is not visible

Gears Legend Gears Legend
Gears Legend

Hello,

for me it seams it can help to change the openGL settings.

For this take also a look to the pictures in the answers at JT2Go Forum.

The settings are the same in Teamcenter Visualisation.

 

https://community.plm.automation.siemens.com/t5/JT2Go-Forum/JT2Go-11-3-0-on-Win10-no-model-visible/t...

 

best regards

Wolfgang

Re: Upgrade TCVis 9 to TCVis 11.3: X_T File is not visible

Siemens Phenom Siemens Phenom
Siemens Phenom

Actually i can't see the version of my X_T-File in File Details.

So next week i'll ask the engineer what X_T Version he created for me.


Open the parasolid text file in any text editor and look/find text similar to "SCH=SCH_2901259_28101"

 

2901 indicates parasolid version as 29.1

259 indicates the build

 

Following is the parasoild information from NX (Just to verify)para.png

 

 

 

Re: Upgrade TCVis 9 to TCVis 11.3: X_T File is not visible

Experimenter
Experimenter

@ Ganesh Kadole:

 

Here is the the Information from the Parasolid X_T opening in Text-Editor:

SCH=SCH_2701211_26105;

 

Thursday i can ask the enineer for checking the file-version in NX (i have no NX installed)

 

Best Regards,
Topptom

Re: Upgrade TCVis 9 to TCVis 11.3: X_T File is not visible

Gears Legend Gears Legend
Gears Legend

Hello,

 

Please let me try to explain the different at the settings between Teamcenter (JT2Go) 9 and Teamcenter (JT2Go) 11. If you change from version 9 to 11 (or 10) the openGL settings are different. Take a look to the attached pictures. Many times is this a problem in Troubleshoot. If the main page looks like a “exploded star” move the button to the right side. After this klick okay and restart the program.

 

Hope this helps.

Folie1.JPGFolie2.JPG

Best Regards

Wolfgang  

Re: Upgrade TCVis 9 to TCVis 11.3: X_T File is not visible

Experimenter
Experimenter

Thanks Wolfgang, now it works - you've described the right way in your Screenshot (Version 11.3)

==========================================

 

Hallo Wolfgang,

 

vielen Dank - es hat bei mir geklappt.

Es war genau dieser Schieberegler in Version 11.3.

Jetzt wird alles wieder angezeigt.

 

Danke & Gruß

========