Cancel
Showing results for 
Search instead for 
Did you mean: 

Referencing Catia (or other CAD) masters in NX master asemblies

Experimenter
Experimenter

So we have a widget group designing and releasing in Catia w/TC integration with "123456" number, I want to reference 123456 in NX form so we can release the parent assembly with "234567" number. Is there a smart method for managing this scenario built into TC?

Steve
Automotive
TC10/NX9
1 REPLY

Re: Referencing Catia (or other CAD) masters in NX master asemblies

Solution Partner Honored Contributor Solution Partner Honored Contributor
Solution Partner Honored Contributor
Usually, whenever multi-cad is involved, you pick a "master" cad system. The other cad systems generate JT's that are then brought into the "master" for assembly. NX is a great choice as the "master".

Randy Ellsworth, Teamcenter Architect, Applied CAx, LLC
NX 11 | SW 2016 | Creo 4 | TcUA 11.4
Evaluating: AW 3.4