Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

Releasing Files

Genius
Genius

Hi.

 

We have a lot of .tif drawings that we will be adding to TC.

 

Is it possible to set the workflow to multiple files to released in one go?

 

Kind regards

 

Darren.

5 REPLIES 5

Re: Releasing Files

Gears Phenom Gears Phenom
Gears Phenom

Good afternoon, try using handlers:

 

EPM-create-status
https://docs.plm.automation.siemens.com/tdoc/tc/11.2.3/help#uid:xid1256819:index_workflow_designer:i...

EPM-set-status
https://docs.plm.automation.siemens.com/tdoc/tc/11.2.3/help#uid:xid1256819:index_workflow_designer:i...

 

For the EPM-set-status handler, notice the -status_not_shared argument

Re: Releasing Files

Gears Phenom Gears Phenom
Gears Phenom

Addition:
You can take the TCM Release Process as an example, add the -status_not_shared argument to the EPM-set-status handler.

 

2019-03-25 13 42 14.png

Re: Releasing Files

Genius
Genius

Hi @ArthurRM 

 

Looks complicated.

Do you know if there is a walkthrough guide anywhere?

 

I would do it at a folder at a time.  These folders will have up to 2,500 til files.

 

Kind regards

 

Darren.

Re: Releasing Files

What method are you using to import the image files?   Using PLMXML import, you could attach the status as part of the import...

Re: Releasing Files

Gears Phenom Gears Phenom
Gears Phenom

Good afternoon, Darren, I created a process for you, you can run it on a folder, all the objects inside the folder will be released.
You can change the status name in your text editor:

2019-03-26 11 00 29.png


Import the process into Workflow Designer:

2019-03-26 10 47 26.png

 

You can also use the release_man utility, but it assigns one status instance to all objects:

 

https://docs.plm.automation.siemens.com/tdoc/tc/11.2.3/help#uid:release_man