Cancel
Showing results for 
Search instead for 
Did you mean: 

SAP und T4S

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor

Hi,

 

Multiple logons with the same username are supposed to be in the near future in a company X suspended.

 

The users have 2-Tier architecture installed on their clients.

 

Will it be possible for the users to log on to the T4S-SAP too? Does logging in to the T4S count as an additional Log?

 

Thanks in advance,

M.

1 REPLY

Re: SAP und T4S

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom
You'll need to check the license file. Find the INCREMENT lines and look for the value of DUP_GROUP. The Duplicate Grouping parameter is optional so it may not be listed. If its missing then the feature doesn't support duplicate grouping. If it is listed then the value will tell you which duplicate groupings are supported.
DUP_GROUP=NONE|SITE|[UHDV]
U=DUP_USER
H=DUP_HOST
D=DUP_DISPLAY
V=DUP_VENDOR
Any combination of UHDV is allowed, and the DUP_MASK is the OR of the combination. For example `DUP_GROUP=UHD' means the duplicate grouping is (DUP_USER|DUP_HOST|DUP_DISPLAY), so a user on the same host and display will have additional uses of a feature not consume additional licenses.

Randy Ellsworth, Teamcenter Architect, Applied CAx, LLC
NX 11.0.1.mp01 | SW 2016 | TcUA 11.2.3
Evaluating:AW 3.2