Cancel
Showing results for 
Search instead for 
Did you mean: 

SCHEDULE MANAGER

Experimenter
Experimenter

I'm new in using TeamCenter Schedule Manager, is here anyone who can help and give some advices and answer my questions?

4 REPLIES

Re: SCHEDULE MANAGER

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom
Yes

Randy Ellsworth, Teamcenter Architect, Applied CAx, LLC
NX 11.0.1.mp01 | SW 2016 | TcUA 11.2.3
Evaluating:AW 3.2

Re: SCHEDULE MANAGER

Experimenter
Experimenter

I create schedules for my cooperators. Mainly there is one design engineer and one process engineer in one schedule, but there are also some engineers who participate into few schedules at the same moment (they are for special process or inspection). How can I adjust schedules to everyone can have maximum 100% load? Currently special engineers have even 300% load because they participate into 5 schedules in the same time and tasks overlap. I tried create cross schedule depedency but when we have 200 tasks or more in one schedule, there is a big problem to do this. Could You help me solve this problem?

Thank You

Re: SCHEDULE MANAGER

Experimenter
Experimenter

Hi,

 

Does a separate license required for Schedule Task to underlying workflow auto triggering Or the basic license of TC030301 (prog_exec_user) is enough ?. We are seing an error message in the syslog file that prog_exec_access license does not exist while attempting the automatic workflow triggering through Schedule task when the task hits the start date. Please clarify.

 

Thanks in Advance,

 

Regards,

Krishna k

Re: SCHEDULE MANAGER

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom
Review the flexlm log for "UNSUPPORTED" or "DENIED" entries to answer your question.

Randy Ellsworth, Teamcenter Architect, Applied CAx, LLC
NX 11.0.1.mp01 | SW 2016 | TcUA 11.2.3
Evaluating:AW 3.2