Cancel
Showing results for 
Search instead for 
Did you mean: 

Selecting User Roles in Teamcenter

Creator
Creator

Hey everyone

 

Is there a user preference that can be enabled to make teamcenter look at all roles available for a user as apposed to having to manually switch between roles when doing tasks?

 

Thanks in advance

 

Ben

9 REPLIES 9

Re: Selecting User Roles in Teamcenter

Solution Partner Esteemed Contributor Solution Partner Esteemed Contributor
Solution Partner Esteemed Contributor

None that I'm aware of.


Randy Ellsworth, Teamcenter Architect, Applied CAx, LLC
NX 11 | SW 2016 | Creo 4 | TcUA 11.4
Evaluating: AW 3.4

Re: Selecting User Roles in Teamcenter

Legend
Legend

There used to be an environment variable AM_MODE. If you set to ON it would check if you have given role without manually switching it.

 

Not sure if the variable is still active. If I find something, I will post.

---

Thanks and Regards

Yogesh Fegade

Re: Selecting User Roles in Teamcenter

Legend
Legend

I was mistaken. That variable is still there, but it pertains to groups and not roles.

 

You may want to see if AUTHORIZATION_MODE will work for you:

 

AUTHORIZATION_MODE

Evaluates all of a user's group and role-in-group settings to determine the effective authorization rules for the user. If left unset, the system evaluates only the current logon settings.

---

Thanks and Regards

Yogesh Fegade

Re: Selecting User Roles in Teamcenter

Creator
Creator

Thanks Everyone

 

Always a wealth of knowledge on this board.

 

Cheers

 

Ben

Re: Selecting User Roles in Teamcenter

Experimenter
Experimenter

In my role, I used to setthe user to an user state, the role can only be used for certain purposes. although he/she exsits they cannot carry out any functions. (set up for FDA purpose) I have traceability intact and the tracts. Also LDAP helps on the way this is setup. (learned this from applying technique from other PLM/PDM applications.

Re: Selecting User Roles in Teamcenter

Solution Partner Esteemed Contributor Solution Partner Esteemed Contributor
Solution Partner Esteemed Contributor

Another preferences related to workflow is SIGNOFF_required_group_and_role. Setting to "0" (default) allows the effective ACL's to perform the signoff instead of "1" where they must be signed in as the correct group/role to perform the signoff.


Randy Ellsworth, Teamcenter Architect, Applied CAx, LLC
NX 11 | SW 2016 | Creo 4 | TcUA 11.4
Evaluating: AW 3.4

Highlighted

Re: Selecting User Roles in Teamcenter

Experimenter
Experimenter

What about this simple preference

TC_current_role
DESCRIPTION
Specifies whether the user’s membership in a role enforces access to objects.
VALID
VALUES
true A member of the role has access to an object only when the role is that user’s
current role.
false A member of the role has access to an object even when the role is not the
user’s current role.
DEFAULT
VALUES
false

Re: Selecting User Roles in Teamcenter

Experimenter
Experimenter

how to set  the environment variable AM_MODE  ? I can not find in tc_help......

Re: Selecting User Roles in Teamcenter

Solution Partner Esteemed Contributor Solution Partner Esteemed Contributor
Solution Partner Esteemed Contributor

AM_MODE is listed in the preferences guide...

AM_MODE.PNG


Randy Ellsworth, Teamcenter Architect, Applied CAx, LLC
NX 11 | SW 2016 | Creo 4 | TcUA 11.4
Evaluating: AW 3.4