Cancel
Showing results for 
Search instead for 
Did you mean: 

Shared session of RAC in custom utility

Siemens Experimenter Siemens Experimenter
Siemens Experimenter

Is it possible to have a custom SOA utilty to use the same session of running RAC? 

 

At present customer is running below command from a shell script which is launched from there ecad application. It is for Teamcenter Enterprise.

omfcl PdmSession abc.exe parameter1 parameter2 parameter3

The pre request of running above command is to have OMF classic client running in back ground.

Since we are replacing TC Ent with TC UA, we need a similar solution. Are there any similar framework in TC UA (like omfcl). If not is it possbile to write SOA code to reuse existing RAC session rather than passing user name and password?

 

2 REPLIES 2

Re: Shared session of RAC in custom utility

Solution Partner Esteemed Contributor Solution Partner Esteemed Contributor
Solution Partner Esteemed Contributor
Not that I know of. However, if your true requirement is not passing username and password then TcSSO w/Kerberos would resolve the issue.

Randy Ellsworth, Teamcenter Architect, Applied CAx, LLC
NX 11 | SW 2016 | Creo 4 | TcUA 11.4
Evaluating: AW 3.4

Re: Shared session of RAC in custom utility

Siemens Experimenter Siemens Experimenter
Siemens Experimenter
agree. but there is no SSO in this instance.