Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

Siemens TeamCenter Visualization 11.2 with XenDesktop

Experimenter
Experimenter

Hi All

We are running a series of test's for customers who use Teamcenter and Catia.

The hardware is a HP DL380 Gen9 with 2 Nvidia Grid K2's.

The processor is Intel Xeon 2660 v3 2.6 Ghz

 

The storage is NetApp SSD.

 

We are using XenDesktop 7.9 and XenServer 7.1.

 

The VDI machines are running Windows 7 64 Bit with K240Q grid card and vdi machines are running 8 vcpu's.

We have large size car drawings. Our engineers are designing the model with the Catia and wiewing with Siemens Teamcenter Visualization.

Our issue: when we rotate the model, 2 seconds delay on first click. But after the first click, we have no problems when we want to rotate the model.
Our problem is that during the first click. This delay time increases when the model file grows.

What can we do for this 2-second delay?