Cancel
Showing results for 
Search instead for 
Did you mean: 

Solid Edge Teamcenter Client -- Cannot log in with 2-tier mode.

PLM World Member Phenom PLM World Member Phenom
PLM World Member Phenom

I have a problem where I cannot log in to Teamcenter via. the Solid Edge teamcenter Client in 2-tier mode.  The error message I receive says that my computer is not connected to a network.  I have run the Set Teamcenter Databases utility and defined the 2-tier configuration.  The Rich Client has been installed in 2-tier mode and works just fine.

 

A login is only successful in 4-tier (default) mode.  All the service packs are current.  Has anybody seen this problem?

1 REPLY 1

Re: Solid Edge Teamcenter Client -- Cannot log in with 2-tier mode.

PLM World Member Phenom PLM World Member Phenom
PLM World Member Phenom

After getting my VAR to log a call with GTAC I got a fix for this.  So for anybody in here that is mildly interested the fix is quite simple and follows below.

 

All you need to do is go to the StartTcServer.bat file on your machine and rem out eight lines as described below.

 

From <Install path>Solid Edge ST6\Preferences\StartTcServer.bat

Edit StartServer.bat file under Preference folder as follows.

To add 'rem' (without quotes) for all the lines start with 'if not exist'. Total 8 changes to be done.

 

Existing - from

 

if not exist %TC_ROOT% goto IMANROOT_error

if not exist %TC_DATA% goto IMANDATA_error

if not exist %TC_ROOT%\bin\tcserver.exe goto IMANTCSERVER_error

if not exist %TC_DATA%\tc_profilevars.bat  goto IMANDATA_Tc_Profilevars_error

 

call %TC_DATA%\tc_profilevars

if not defined IMAN_TMP_DIR set IMAN_TMP_DIR=%TC_ROOT%\portal\temp

if not defined IMAN_LOG set IMAN_LOG=%TC_ROOT%\portal\temp

if not defined Transient_Volume_RootDir set Transient_Volume_RootDir=%USERPROFILE%\Local Settings\Temp\TransientDirs

if not exist "%Transient_Volume_RootDir%" mkdir "%Transient_Volume_RootDir%"

 

Change-to

 

rem if not exist %TC_ROOT% goto IMANROOT_error

rem if not exist %TC_DATA% goto IMANDATA_error

rem if not exist %TC_ROOT%\bin\tcserver.exe goto IMANTCSERVER_error

rem if not exist %TC_DATA%\tc_profilevars.bat  goto IMANDATA_Tc_Profilevars_error

 

call %TC_DATA%\tc_profilevars

rem if not defined IMAN_TMP_DIR set IMAN_TMP_DIR=%TC_ROOT%\portal\temp

rem if not defined IMAN_LOG set IMAN_LOG=%TC_ROOT%\portal\temp

rem if not defined Transient_Volume_RootDir set Transient_Volume_RootDir=%USERPROFILE%\Local Settings\Temp\TransientDirs

rem if not exist "%Transient_Volume_RootDir%" mkdir "%Transient_Volume_RootDir%"