Cancel
Showing results for 
Search instead for 
Did you mean: 

Solid Edge automatic STEP file generation in Teamcenter

Experimenter
Experimenter

Has anyone veen able to automatically generate STEP files to save into Teamcenter through the Solid Edge Embedded Client without having to go through Siemens for programming support?

2 REPLIES 2

Re: Solid Edge automatic STEP file generation in Teamcenter

Valued Contributor
Valued Contributor

To the best of my knowledge there is no way of doing this in SE.

Work around is saveas translated then drag and drop dataset back into teamcenter and associate it with your Item.

There is a step translation module that can be purchased as an add-on, but again you would still need to drag and drop the dataset into teamcenter.  This add-on lets you select the dataset in the TC Client --> Tools --> Export --> Objects.  User would then select the application tool (STEP).

Re: Solid Edge automatic STEP file generation in Teamcenter

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor
If You use this translator, you can do translation from command line or You can set Dispatcher to do this translation asynchronous.

"JT Bi-Directional Translator for STEP"

Best regards

Bernard Pacula,
CAMdivision Sp. z o.o.
Consultant PLM/System Architect