Cancel
Showing results for 
Search instead for 
Did you mean: 

Spinoff of pax file failed

Siemens Experimenter Siemens Experimenter
Siemens Experimenter

The pax file nxdm_ugs_manufacturing_templates.pax was moved from UGII\templates to MACH\templates in NX11.0.  The script tcin_cam_template_setup.bat failed to update the pax file due to the location of the pax file was moved.

To duplicate the problem, run the script with -pax option. For example,

tcin_cam_template_setup.bat -u=infodba -p=<password> -g=dba -pax

 

Template update was successful but spin off of pax file failed. I think becuse of location issue.

 

find attached.

1 REPLY 1

Re: Spinoff of pax file failed

Solution Partner Esteemed Contributor Solution Partner Esteemed Contributor
Solution Partner Esteemed Contributor
Have you tried it using "Import Assembly into Teamcenter" method instead of the command line?
Launch Teamcenter and logon as infodba
Select Home folder
Launch NX/Manager
Select Import Assembly into Teamcenter
Default Name = OS Filename
Conversion Rule = As ID
Select Import from Folder, browse to UGII_BASE_DIR\UGII\templates\sample
Select Dry Run, examine the log, Default_Container = :Newstuff
Select Default Destination Folder
Select Create new folder, type NXTemplates
Select OK to install NX templates
Validate contents of NXTemplates folder in Teamcenter


Randy Ellsworth, Teamcenter Architect, Applied CAx, LLC
NX 11 | SW 2016 | Creo 4 | TcUA 11.4
Evaluating: AW 3.4