Cancel
Showing results for 
Search instead for 
Did you mean: 

TC_MFK_DEFAULT_DOMAIN is not set Error when opening NX12.

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor

One of the NX12 users while working remotely (connected through VPN) encountered an error: "The preference TC_MFK_DEFAULT_DOMAIN is not set. NX only supports items in the default domain." when he started NX that uses parameter: -pim=yes. The problem did not appear again when he started RAC first and then NX again.

 

Any idea what could have caused this error? Maybe a unstable network?

 

Thank you in advance!

2 REPLIES 2

Re: TC_MFK_DEFAULT_DOMAIN is not set Error when opening NX12.

Siemens Esteemed Contributor Siemens Esteemed Contributor
Siemens Esteemed Contributor

TC_MFK_DEFAULT_DOMAIN is a TC preference which can be set to varying levels of Protection Scope (user/role/group/site).

 

Could the user have connected to the database with different credentials using -pim than when starting NX from RAC?

Ben Broad | PLM Enthusiast | Siemens GCSS

NX (v17 - 1872) | Teamcenter (9 - 12)
Value Based Licensing | Adaptive UI | BETA Registration

Re: TC_MFK_DEFAULT_DOMAIN is not set Error when opening NX12.

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor
Hello! Thank you for the answer.

I confirmed that he used the same credentials as he logged in to RAC. After he logged through RAC he then opened NX using -pim (Did not open NX from RAC). I suspect that the connection failed somehow, maybe due to unstable network, when he first opened NX using -pim. So when he started the RAC the connection was established without errors and was able to login through -pim without errors. The person has a NX shortcut that has the -pim parameter.