Cancel
Showing results for 
Search instead for 
Did you mean: 

TC1015 JAVA API whereReferenced crashes

Legend
Legend

I get error when using whereReferenced()  JAVA api in 10.1.5

 

Siemens on GTAC recommend patching to 10.1.6

 

Is there alternate method for whereReferenced()? May be with SOA?

 

3 REPLIES 3

Re: TC1015 JAVA API whereReferenced crashes

Legend
Legend

Hello Alex_c,

Have you tried calling a custom saved query? (com.teamcenter.services.strong.query or its loosely typed version alternative)

Re: TC1015 JAVA API whereReferenced crashes

Phenom
Phenom
In SOA .Net I see a method WhereReferenced() under DataManagementService. There should be a similar function for Java as well.

Re: TC1015 JAVA API whereReferenced crashes

Legend
Legend

Sure there is, it is the DataManagement from the core library (com.teamcenter.services.strong.core). But it is most probably calling the same background function as the one that is causing the failure. That is why a query-based workaround was suggested.(com.teamcenter.services.strong.query).