Cancel
Showing results for 
Search instead for 
Did you mean: 

TCUserService is obsolete in TC10 ?

Legend
Legend

Is TCUserService.call work in TC10? Or starting with TC10 I have to use only SOA methods for that and also migrate my custom_exit to newly created SOA library?

1 REPLY

Re: TCUserService is obsolete in TC10 ?

Siemens Phenom Siemens Phenom
Siemens Phenom

Got this from GTAC: 

 

However User Services is a legacy way to call custom server code from only the rich client.  The capability to define new User Services is deprecated and will not be supported in new Teamcenter Clients ( TCUserService.call method combined with the USERSERVICE_ is deprecated in tc10.x and obsoleted in tc11.x) 
Existing User Service implementation will continue to be supported for legacy code.

In later releases of teamcenter, SOA services would be the way to go.