Cancel
Showing results for 
Search instead for 
Did you mean: 

TcVis 11 from Teamcenter Webclient

Experimenter
Experimenter

Hello Everyone,

 

i have a small problem. I try to open an Document from Teamcenter Webclient and get the following message ( Picture ).

 

TcVis 11.2 Base Version include Mokka is installed.

 

 

 

Chriss

3 REPLIES

Re: TcVis 11 from Teamcenter Webclient

Solution Partner Honored Contributor Solution Partner Honored Contributor
Solution Partner Honored Contributor
Unlike the rich client which includes the base version of Teamcenter Visualization by default, the web client requires that Teamcenter Visualization be installed before you can use the embedded viewer. Just like the rich client includes TCCS/FCC but the web client requires to TCCS/FCC only installed.

Randy Ellsworth, Teamcenter Architect, Applied CAx, LLC
NX 11 | SW 2016 | Creo 4 | TcUA 11.4
Evaluating: AW 3.4

Re: TcVis 11 from Teamcenter Webclient

Experimenter
Experimenter

Good Morning Randy,

 

thank you for your answer. TcVis 11.2 Base is installed on the Workstation but still i gett this message. Is the Base version not enough ??? .

 

 

Christian

Re: TcVis 11 from Teamcenter Webclient

Solution Partner Honored Contributor Solution Partner Honored Contributor
Solution Partner Honored Contributor
That depends on the type of object you're trying to view. If you can view it in the rich client then you should be able to view it in the web client. I won't be able to take you much further with debugging TcVis. Future questions get much harder.

Randy Ellsworth, Teamcenter Architect, Applied CAx, LLC
NX 11 | SW 2016 | Creo 4 | TcUA 11.4
Evaluating: AW 3.4