Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

Teamcenter 11 & Creo 3.0 Issue

Experimenter
Experimenter

Hi All, 

 

im new here, did a quick search but couldnt find my solution.

 

Problem - If i have for example "Part A" on my local hardrive, i check it in, someone else checks it out, modifies it and checks it back in.... i then check it out and load "Part A" from Teamcenter, however it loads my local file instead of the updated one on teamcenter, if that makes sense?

 

Is there an option where when i check it out it loads/overwrites my local version with the team center file?

 

Thanks

1 REPLY 1

Re: Teamcenter 11 & Creo 3.0 Issue

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor

Hi,

 

the only solution that I found was Erase not Displayed and clearing the Cache Manager in Teamcenter toolbar.

For Erase not displayed you can create map key but for Cache manager map keys are not working as it could so you have to do it manualy.

 

Capture.PNG

 

It is not a perfect solution but it was the only that I found when I did the Creo integration.